Smart health appliances

We make smart health appliances work

Supporting health & well-being

Infineon's semiconductor products and software solutions are the perfect match for smart health appliances as they meet the needs of digital healthcare devices. We support a health-conscious lifestyle by enabling smart devices that can help improve well-being and stay healthy longer by making them reliable, convenient, personalized - and secure. That's our contribution to a functioning healthcare system facing a rising global population and aging.

Good health increasingly means taking responsibility of our long-term preventive care rather than sporadically treating acute illnesses. It places great emphasis on enhancing well-being to prevent illness. And it recognizes the role of the home as an important factor in individual health improvement and, in the event of illness, care.

With technologies such as sensors, microcontrollers, actuators, connectivity modules, security solutions together with software, the IoT has great potential to prevent diseases and improve health. There are innumerable health wearables and fitness devices able to track key health markers, such as a user’s heart rate or breathing patterns, that may afford users greater awareness of their health and allow them to make pro-active decisions regarding their health and well-being. 

Vital sensing system

Supporting an Aging Society

The Millimeter Wave Radar Biometric Detection System, developed by a Japanese company called Fingal Link, is a system for monitoring the elderly that is designed to be installed in nursing homes and residential living spaces. It operates by continuously monitoring various health parameters, including blood pressure, heart rate, and sleep quality, in a non-contact manner throughout the day. The collected data is then securely managed in the cloud. This system utilizes Infineon's 60GHz radar IC to achieve its objectives.

The Millimeter Wave Radar Biometric Detection System

What kind of product is the Millimeter Radar Biometric Detection System?

  • It is installed in the living rooms of nursing homes and residences and measures the subject's blood pressure, heart rate, sleep quality, and other parameters 24 hours a day in a non-contact manner.
  • The measured information is managed in the cloud.
  • The solution uses Infineon's 60GHz radar IC.

What kind of sensor is the millimeter wave radar installed in the system?

  • Radar emits radio waves, receives reflections from the object, and obtains various information from the difference between the two.
  • Infineon provides a selection of a radar solutions, including 24 GHz microwave radars and 60 GHz millimeter wave radars.
  • Benefits of the 60 GHz millimeter-wave radar are high detection accuracy and wide frequency swing 
  • It provides non-contact biometric information without privacy concerns typically associated with continuous image capture by cameras.

In the context of advancing technology's impact on various industries, Infineon's innovative radar system holds significant promise for the future, particularly in the healthcare and elderly care sectors. While Infineon has been a key supplier of semiconductors to industries like automotive and consumer electronics, the full potential of technology in medical and nursing care remains largely untapped. The integration of IoT technology through systems like our radar solution can have far-reaching implications in an aging and depopulated society.

The IoT-based systems enable remote monitoring of elderly individuals in rural areas, alleviating the burden on caregivers and enhancing the quality of care services. This technology has the potential to significantly improve elderly care and contribute to an enhanced quality of life for the aging population through advanced technology.

The future of health and well-being

Convenient, smart, and secure

Clearly, the pandemic has driven digital developments at a rapid pace, including the medical field. And that is a good thing, because the digitalization of health appliances offers many advantages for everyone - especially since the patients get much more insight.

As the future of health focuses more and more on self-care, customers are spending more on products like smart wearable devices or smart home devices that help to improve their health, fitness, nutrition, appearance, sleep, and mindfulness. And this holds a lot of benefits.

  • Smart wearables like fitness trackers enable patients to create their own overview of important health data and allow them to reflect on this with their doctor and derive appropriate, preventive actions.
  • The understanding and acceptance of treatments using digital applications has changed fundamentally - decisions are becoming less top-down and more eye-to-eye.
  • Health data can be collected and transmitted directly to the doctor via digital applications – for example, in the case of diabetes and high blood pressure. This makes it more efficient and leads to faster results for patients - of course, without losing sight of data security in the process

Enabling new smart health and fitness technologies

As stated in the WHO Health Promotion Glossary of Terms, health promotion is the "process of enabling people to increase control over, and to improve their health". Infineon’s portfolio of innovative and state-of-the-art semiconductor solutions support:

  • the design of innovative technologies and devices for smart health monitoring, for example medical wearables
  • preventive healthcare appliances like sleep monitoring
  • and, in the event of illness: solutions for assisted living at home

Sensors, connectivity technologies and security solutions enable massive improvements in secured, efficient, convenient and patient centered health and well-being solutions as well as services for patient engagement. The expected growth in sales of semiconductors for medical electronics is estimated at 64% until 2026.

The global IoT market trend in medical devices is clearly moving towards "healthcare is self-care" with a focus on active patient engagement and patient-centric care. The vital signs monitors segment is expected to grow at the highest rate. Let's take smart health appliances like fitness wearables as an example: A medical band tracks health and fitness data and enables an efficient monitoring for individuals, doctors and medical staff. Particularly valuable in critical situations: In the event of conspicious irregulations, the medical band can advise users to take a certain action first, for example, to take a medication. If serious irregularities develop, the doctor can be contacted or an emergency call can be alerted.

Even though medical devices consist of a lot of technical know-how, the focus of smart health devices is always on people and their needs. It is about empowering people to have a better and healthier life.

More to ... semiconductors for smart health appliances

SENSE: Sensors are the basis for measuring the state of health

The XENSIV™ family is the broadest portfolio of sensor types on the market, offering smart-device manufacturers turnkey solutions that enable a fast time-to-market.

XENSIV™ MEMS microphones introduce a new performance class for MEMS microphones. The portfolio of XENSIV™ MEMS microphone-based reference designs and Infineon inside MEMS microphones will propel audio performance to the next level for even the most demanding applications.

The XENSIV™ family comprises digital, barometric absolute pressure sensors that impress with their small size, low power consumption, highest precision, environmental robustness and relative accuracy over a wide temperature range. Explore our Infineon inside pressure sensor partner products to find the ideal solution for your needs.

Health monitoring, gesture control, and presence detection are among the applications for which Infineon’s 60 GHz radar is a versatile solution, while Infineon’s REAL3™ image sensors are the right choice for authentication via face recognition and AR/VR applications. They are based on Infineon ToF (time of flight), which is the most advanced vision-sensing technology in the world today.

Yet smart things also rely on physical interaction between users and devices. Infineon’s CAPSENSE™ solutions bring elegant, reliable, and easy-to-use capacitive-touch sensing functionality to your design. CAPSENSE™ boasts industry-leading low-power operation, with an average current consumption of 22 µA.

COMPUTE: Microcontrollers and high-performance memory solutions bridging the gap between high performance and low power

PSoC™ 6 bridges the gap between expensive, power-hungry application processors and low performance microcontrollers (MCUs).

The PSoC™ 6 MCU contains a dual CPU architecture, with both CPUs on a single chip. Beyond the low-power core, the PSoC™ 6 programmable processor line has six power modes for fine-grained power management. Built-in security protects your IoT system.

Matching the PSoC™ 6 family, EXCELON™ – the next-generation Ferroelectric RAM – combines ultra-low-power operation with high-speed interfaces, instant nonvolatility, and unlimited read/write cycle endurance, making it the ideal data-logging memory for portable medical, wearable applications.

We expect our smart things to work anytime, anywhere. At the same time, they should offer maximum safety, reliability, and security. Rely on our broad portfolio of safe, secured, and reliable solutions for embedded systems for embedded systems and check out our NOR Flash products.

ACTUATE: From Qi transmitter to Class D amplifier

Wireless power is becoming increasingly integral for the multifaceted world of smart things. Infineon offers safe and efficient wireless charging solutions for inductive and resonant topologies.

These include customized turnkey system solutions containing software, such as the 15 W Qi table-top transmitter or the 2.5 W resonant multi-device charger with transmitter and receiver solutions.

For great-sounding products, Infineon's MERUS™ multilevel Class D amplifier ICs boast superior energy efficiency and power density. Infineon’s portfolio includes fully integrated single-chip audio solutions alongside discrete audio solutions with highly scalable amplifier driver IC and power MOSFET combinations.

CONNECT: From Bluetooth to 5G - Connectivity on demand

Today’s requirements for mobile-device and wireless applications are increasingly strict due to 4G/5G. Designers therefore need highly integrated RF front-end solutions with lower loss rates, more powerful performance, and greater linearity. Infineon offers a broad product portfolio of high-performance RF front-end components, including antenna tuners, RF switches, LNAs, and LMMs.

To ensure flexible connectivity worldwide, Infineon offers a wide range of high-quality 5G-ready eSIM solutions ranging from eSIM hardware to high-end, ready-to-connect bundles like OPTIGA™ Connect. Combining certified, best-in-class security hardware with a fast, interoperable operating system (OS), OPTIGA™ Connect solutions are optimized for the requirements of the IoT and consumer devices. Pre-integrated connectivity and remote profile provisioning capabilities support fast and easy deployment and management of connected devices the world over.

The WICED Wi-Fi + Bluetooth combos are a small-form-factor solution for IoT designs and integrate IEEE 802.11a/b/g/n/ac WLAN and Bluetooth into a single-chip. Many of the Wi-Fi + Bluetooth combos are supported on WICED Wi-Fi and ModusToolboxTM software development kits that provide code examples, tools, and development support.

SECURE: Creating trust in the digital world of healthcare and medical devices

One-stop security solutions from Infineon turn a smart thing into a versatile wallet.

SECORA™ Connect is an all-in-one, turnkey solution that turns the respective wearable or IoT device into a powerful and versatile wallet for securely storing, selecting, and using multiple payment cards or transport tickets, for instance. SECORA™ Connect allows designers of smart wearable systems with no security or antenna design experience to seamlessly integrate a very compact solution with ultra-low power consumption for various NFC-based applications.

SECORA™ Blockchain is a fast, easy-to-use Java Card™ solution boasting best-in-class security for blockchain system implementation. By providing a safe “vault” for user credentials, SECORA™ Blockchain can reduce the end user’s commercial risk and helps to increase trust in the blockchain system.

Last, but not least, the OPTIGA™ Trust, OPTIGA™ Authenticate and OPTIGA™ Connect product families offer a full range of security chips to address individual needs in the field of embedded authentication, brand protection, and advanced security applications.

Easy and intuitive health monitoring everywhere

Health and fitness wearables

Today’s hyperconnected consumer wants one thing above all else – convenience. Easy, intuitive ways to tune into the useful information they need. The global market for smart devices is expected to increasingly focus on active patient engagement and patient-centric care. Small, smart, wearable devices play an important role in this area as they automatically and regularly measure health values - for the patient's own control or for a doctor's control.

Health and fitness wearables such as smartwatches, sports watches, fitness trackers and healthcare wristbands can be comfortably and discreetly worn on the body and support a growing number of use cases, including health and fitness tracking. Equipped with health monitoring functionalities, wearables can measure physical activity and vital parameters such as heart rate, blood pressure or blood oxygen levels. Potential risks can thus be identified at an early stage and solutions can be quickly targeted. However, they do not replace visits to the doctor – the focus is rather on preventive options and health monitoring. Wearables can even tell if the wearer has fallen. By supporting connected health, they enable elderly people in particular to live independently and safe.

Learn more about the technology behind innovative solutions supporting health and well-being:

In addition to the “classic” wearables for measuring fitness values like smartwatches, sport watches or fitness tracker, more and more new, innovative formats such as rings or other jewellery, are entering the market. Smaller, more inconspicuous, more individual, they pose great challenges to manufacturers in terms of storage capacity, battery life, handling, precision, reliability, security, etc. Users expect a beautiful design with the same or even better functionality and reliable and easy handling.

Oura Ring. Smart ring for fitness, stress, sleep & health monitoring.

The Oura Ring is an innovative wearable that helps you monitor and improve health. Sleep, readiness, and activity - these scores tell you how your body feels and what your body needs, every second of every day. You'll know when you need more sleep, when you might be getting sick, when it's time to push yourself - and more - with a personalized experience on the Oura App.

The Oura Ring requires long-lasting battery life, increased processing capacity, and the use of advanced sensors, all in a stylish and comfortable form factor. This innovation is delivered through PSoC™ 6 MCUs, enabling the following features:

  • Small form factor: Integration of several functions into a single PSoC™ 6 MCU helped reduce the size of the ring over the prior generation by 50%.
  • Data storage: PSoC™ 6’s on-chip flash memory enables storage of up to six weeks of user data.
  • Bluetooth low energy: The built-in BLE wireless connectivity in PSoC™ 6 provides communication to the mobile app device.
  • Extended battery life: PSoC™ 6’s ultra-low power was able to extend battery life to seven days, 3X longer than the prior generation ring.
  • Sensor fusion: PSoC™ 6, as the host processor, connects different biometric sensors in the ring to collect and process data.
  • Data processing: The dual Cortex-M4 and Cortex-M0+ cores in PSoC™ 6 enabled 10X more processing capability vs. the prior generation ring

Wrist-worn health bands are becoming more and more popular among elderly people. Medical bands offer a range of health-monitoring features that keep users updated about their health status in real-time. In addition to general health and activity tracking, they can also help users to manage underlying diseases or chronic conditions by connecting with telehealth services and transmitting specific health metrics such as heart rate, blood pressure, and blood sugar levels to a healthcare provider of their choice. Location and fall detection can add another safety net. All of which can enable elderly people to live safely and independently – for longer.

Everything it takes for safe, secure and reliable healthcare bands

Click here to learn more about our extensive portfolio covers all sensing, computing, memory, power and connectivity building blocks needed to create safe, reliable wrist-worn healthcare devices.

Health monitoring @ home

Solutions for the smart home

The increase in chronic diseases and health problems in our society often entails the need for home care or self-treatment at home. The desire for a self-determined life is just as decisive for this as the lack of suitable facilities in some regions. This is where the smart home can help with home automation and health monitoring solutions.

Smart home technologies can provide some simple services while collecting health data that can help people in need of care to reduce their dependence on healthcare providers and improve their quality of life at home. Health monitoring at home also helps to keep an eye on the state of health and, if necessary, to take countermeasures if health values deviate.

Discover innovative solutions supporting health and well-being at home:

There is no doubt about how important good sleep is for physical and mental well-being. The quality of sleep affects how fit and efficient one is during the day. Sleep even affects the risk of developing lifestyle diseases such as obesity, depression and type2 diabetes. Unfortunately, many people struggle with intermittent or even regular sleep problems. Finding out the reason for this often proves difficult. Sleep monitoring can help here to measure the quality of sleep and gain valuable insights into individual sleep patterns. 

Infineon’s next generation radar based XENSIV™ Sleep Quality Service is a fully integrated hardware and software solution for OEMs to help improve people’s sleep.

Radar solutions are a key enabler for the digitalization of medical healthcare in sleep improvement solutions like the solutions of Sleepiz or Tsingray.

The biggest highlight of the Tsingray device is the adoption of millimeter-wave radar tomography sensing technology pioneered in the industry. With 2.5cm resolution chromatography and 100ms refresh period, it can monitor from multiple dimensions such as sleep, breathing, heart rate, body movement, sleeping posture, etc., that is, all the micro-motion data of the monitored person during sleep can be completely recorded.

How do Infineon’s products contribute to this innovative Tsingray solution?

The smart sleep breathing monitoring device, using Infineon’s XENSIV mm-wave 60GHz radar chip, has recently been included in the cooperation of Tsingray with JD Health. This device is now part of a healthcare online service package for sleep quality improvement of "JD.com”, a huge online trading platform based in Greater China. In addition to Infineon’s XENSIV millimeter-wave radar chip, Tsingray is also adopting Infineon's Wi-Fi/BLEPSoC MCU and OPTIGA™ Trust B security chip solutions for the development of next-generation products of this sleep monitor.

With the support of Infineon’s XENSIV 60GHz mm-wave radar chip, the smart sleep breathing monitoring device is capable of realizing:

  • Non-contact and non-sensitive continuous sleep monitoring and collection of real-time data all night long without affecting sleep.
  • Accurate perception of vital signs and body movement micro-data of the whole sleep process, and multi-dimensional sleep monitoring by mm-wave chromatography.
  • Automatic generation of monitoring reports providing data reference for customized sleep improvement plans, expert consultation, follow-up visits
  • Diagnosis of sleep problems by AI auxiliary diagnosis and treatment system.
  • Measurement of distance between objects with mm level precision with lower power consumption and minimal volume.
  • Non-contact monitoring method, which avoids users’ discomfort, making the device very suitable for long-term home monitoring.
  • Timely warning of sudden sleep death omens, long-term apnea and other dangers, which fills the gap of accurate monitoring of nighttime breathing patterns and heartbeat patterns.
  • Support of the diagnosis of chronic breathing diseases such as chronic obstructive pulmonary disease, asthma, apnea and hypoventilation.

With smart speakers becoming the central control hubs of smart houses, presence detection enabled by a radar sensor allows OEMs to provide advanced, innovative features to differentiate their products in this highly competitive and rapidly growing market segment. Adding a radar sensor can improve the user experience by sensing the “real” presence and location of a person. Because it can detect the direction of movement (angle of arrival), the smart speaker for example is now aware that someone is approaching so that it can power up the VUI and internet connection to be ready to listen for commands. There is now no longer a need for a ‘wake up’ word.

Health monitoring features for smart speakers enabled by radar sensors

The amazing sensitivity of a radar sensor enables smart speakers to have new features for health monitoring. This is an exciting new area that address the growing awareness of the importance of health monitoring as can be seen by fitness trackers and the features built into smart watches such as exercise, sleep and heart monitoring. Thanks to a radar sensor’s sensitivity, which can even detect a pulse in a wrist, there are now many health monitoring opportunities that can be designed into a smart speaker with a radar sensor to add user value with hardly any impact on the system costs as these are all in software.

Examples are the use cases of fall detection, unobtrusive monitoring of elderly people who unexpectedly change their daily routines so that they can be checked in case of a problem, monitoring of respiration rate, irregularities in heart rate patterns as an early warning of a possible problem, and even coughing or snoring. All of which can be done automatically eliminating the problem when the elderly person forgets to wear the monitoring device. 

With the recent pandemic, awareness of indoor air quality is rising. At the same time, energy-efficiency is an important topic of our time. Efficient building insulation can help save energy - but heavily insulated homes are not always good for health. Poor ventilation can lead to lower oxygen levels and a buildup of carbon dioxide (CO2). Even moderate CO2 levels can have a negative impact on health and productivity - people become drowsy and have difficulty concentrating. So the demand is growing for smart indoor air quality sensors that can "smell" rising CO2 levels and either warn the user or trigger a system response. Real-time CO2 monitoring for demand-controlled ventilation systems, air purifiers and thermostats allows users to accurately measure and adjust indoor air quality.

eesy-innovation launches an easy-to-use consumer CO2 sensor to improve health and mental well-being

In the light of the COVID-19 pandemic and overall increased health concerns, co2go® is the answer to a growing need and demand for CO2 sensors in the end user market space. The innovative mobile CO2 sensor, developed by our Associated Partner eesy innovation, is able to measure the levels of CO2 indoors wherever you are. The co2go® may be easily linked to a smartphone or laptop, and it offers transparency through information about the quality of the air in your immediate surroundings - enabling you to optimize your health and mental well-being. The CO2 level is indicated through a traffic light display on the device itself. Additionally, a dedicated Desktop App is available via the connected laptop.

The co2go® device is easy-to-use and enables consumers to protect themselves from an invisible hazard in the air – heightened CO2 levels. This sensor can be used wherever there are people gathering in a closed space, such as classrooms, offices, meeting rooms, restaurants, or simply at home.

Unlike previous CO2 devices that use an indirect measurement method like electrochemical methods (EC), infrared light (NDIR) or equivalent carbon dioxide (eCO2), co2go® uses the superior technology of Infineon´s new XENSIV™ PAS CO2 sensor and can quantify CO2 levels directly through photoacoustic spectroscopy (PAS).

In comparison to products available before and thanks to Infineon’s innovative sensor technology, the co2go® features an outstanding measurement accuracy with a very small footprint. Previous size, performance and cost restrictions could be eliminated. This technological breakthrough paved the way to the mobile small form factor for an everyday, personal, and portable health assistant device.

Protecting sensitive health data

Healthcare privacy and security

In recent decades, the use of digital technologies in health and lifestyle has advanced exponentially. The potential applications are many: imaging for diagnosis, electronic health cards, robotics in surgical procedures, telemedicine, home and mobile monitoring devices to monitor the health of individuals. This increase in digitalization makes the safeguarding of health and patient data urgent and is a basic requirement for the functioning of the digital health system.

With topics such as Artificial Intelligence (AI), Machine Learning (ML) and Big Data also playing an increasingly important role, it is becoming essential to secure data to prevent the misuse of private and sensitive information.  

Our solutions to secure sensitive health data

Equipping smart health appliances with the right security solutions from the get-go is key to helping prevent attacks – whether theft, fraud or manipulation. Companies who are looking for a security solution need one that is equally easy to use – in terms of fast integration and time to market – and trustworthy. Unlike software-only solutions a hardware-based solution is strong, tamperproof and provides a solid foundation. Infineon's independently-certified hardware security solutions are pre-integrated and therefore easy to integrate into your system. The OPTIGA™ Trust and OPTIGA™ Authenticate S solutions protect the storage and transfer of highly sensitive personal healthcare data.

Worldwide, healthcare fraud costs insurance authorities and companies hundreds of millions of dollars every year. With conventional systems based on paper or memory cards, it is difficult for authorities to ascertain whether the patient or user is actually the insured.

Enhancing fraud prevention with electronic health cards

While electronic health cards promise greater convenience and an improved patient experience, e-health cards must ensure that personal medical records do not fall into the wrong hands.

Electronic health cards are becoming an increasingly effective way of preventing fraud – particularly as they evolve towards more sophisticated identification mechanisms such as biometrics. E-health cards have the potential to improve the patient experience by storing key medical data and medication history, and by serving as an electronic prescription. These cards can also be used to securely store social security numbers.

Given the sensitive nature of medical data stored on e-health cards, they must offer robust protection of privacy. Widespread adoption also calls for ease of administration and – most importantly – a mature telematics infrastructure to network all players in the care continuum and enable dynamic updates of data and functionality.

Leading technologies for tomorrow’s eHealth cards

Customers value in particular the ability of our controllers to protect sensitive data, while delivering the memory, performance and cost efficiency required for future-proof electronic health cards. The SLE 78 features Integrity Guard, for instance, a self-checking dual CPU which not only stores, but also internally processes sensitive data in encrypted form.

Designed specifically to ease security implementations and certification processes, Integrity Guard combined with our SOLID FLASH™ memory radically reduces cost of ownership by accelerating time to market.

For ease of deployment, we also deliver fully integrated software solutions on native or on Java platforms.

Definition and facts

What are smart health appliances?

Just a few years ago, digitalization in healthcare may sounded distant, but it is already in full swing now. Smart health appliances such as fitness tracker and smart watches can record and document data in real time. Important medical appointments can be set up digitally to help efficiently from any location. Decision-making and self-care behaviors are digitally supported and encouraged like never before. All of this enables patient engagement to support healthiness and well-being what will become increasingly important in the future.

Why it that?

We live in a world of rising population. The latest projections by the United Nations suggest, that the global population could grow to around 8.5 billion in 2030 and 9.7 billion in 2050. At the same time, life expectancy is increasing and will reach a global average of 77.2 years in 2050 (1)

This development presents us with challenges: Everybody wants to live healthy, vital, and as independently as possible into old age. According to the United Nations Sustainable Development Goal No. 3, for sustainable development it is imperative to ensure health and well-being across all ages(2). In order to achieve this and prevent a collapse of the healthcare system, the topics of preventive healthcare, self-care and well-being are becoming more important. A key factor in achieving this is digitalization and the Internet of Medical Things (IoMT), also called healthcare IoT.

  1. United Nations Department of Economic and Social Affairs, Population Division (2022): World Population Prospects 2022: Summary of Results. UN DESA/POP/2022/TR/NO. 3.
  2. United Nations: Sustainable Development Goals; https://unric.org/en/sdg-3/